AXIS#.SAFEPARAM.SSR_#.DECLIMIT

Description

Indicates the deceleration limit of the deceleration monitoring of the Safe Speed Range (SSR) safety function. The deceleration monitoring needs to be enabled in the safety parameters (see AXIS#.SAFEPARAM.SSR_#.DECMONITOREN). A value of zero means the deceleration monitoring is disabled.

 

Context

For complete SSR information refer to SSR (Safe Speed Range).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

Depends on user units

Range

0 or [1, 2^31-1]

Default Value

0 (Disabled)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SSR_1.DECLIMIT

3161h

05h

Unsigned32

-

-

Read/Write

No

AXIS1.SAFEPARAM.SSR_2.DECLIMIT

3162h

05h

Unsigned32

-

-

Read/Write

No

AXIS1.SAFEPARAM.SSR_3.DECLIMIT

3163h

05h

Unsigned32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_1.DECLIMIT

3261h

05h

Unsigned32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_2.DECLIMIT

3262h

05h

Unsigned32

-

-

Read/Write

No

AXIS2.SAFEPARAM.SSR_3.DECLIMIT

3263h

05h

Unsigned32

-

-

Read/Write

No